Dear All.
We use Sabre(i.MX53) with IMX53_WCE700_1105_BSP_SOURCE.
We have to use 10Mbps communication on Ethernet of Sabre.
Can we need to modify BSP ?
1.Please set 10Mbps/FullDuplex or HalfDuplexof PCs network port.
2.Please connect a cross or straight cable Sabre and PC.
3.The link status on PC will be 10Mbps/Full or Half.
4.Ping command does not pass from PC or Sabre.
5.Ping command pass on 100Mbps connection.
BR
Yoichi
DeaD
Please check the WINCE700 Reference Manual, in Chapter 15 you would find the instructions to add the FEC driver to the BSP and the changes required in the registry in order to get the FEC Driver Upload. By default this is enable asyou can review in the documentation. So It maybe a problem in your Eboot with your MAC Address setup or you IP Number. that you are using.