AnsweredAssumed Answered

U-Boot Video Parameters for SEIKO-WVGA on i.MX6

Question asked by squirem on Jun 27, 2013
Latest reply on Feb 24, 2014 by Yixing Kong

I'm using the SEIKO 4.3" WVGA touchscreen display on an i.MX6 board. I'm using the SabreSD development board and connects through an LCD expansion connector. The board is running a Linux image generated by the Freescale Yocto BSP. For reference I've been appending these video parameters:

video=mxcdi0fb:RGB24,SEIKO-WVGA

to the mmcargs environmental variable.


However, this does not seem to work. I'm wondering if anyone has previously used this display module with the SabreSD board or the i.MX6 platform?

Outcomes