CCSprotocolPlugin: failed to correctly configure JTAG chain - For Simulator Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCSprotocolPlugin: failed to correctly configure JTAG chain - For Simulator Project

952 Views
vijaykishore
Contributor III

I am using Code Warrior version 10.3 evaluation version.

We don't have a target board now.

So, I am trying to create a Simulator project.

For this I have selected P4080 processor.

I didn't modify any code after creating the project.

(There were some printf's in the main.c of Sources folder).

 

So, I just compiled the code. It happened successfully. And now when I tried to run, an error occured.
The issues which I faced are attached here as screenshots (as P4080_Simulator1 and P4080_Simulator2).

 

The procedure which I followed for creating, building and running a project is attached below as P4080_CW_SShots.doc.

Labels (1)
Tags (3)
0 Kudos
0 Replies