CodeWarrior V6.4 for ColdFire; Flash Programmer can't calculate checksum.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior V6.4 for ColdFire; Flash Programmer can't calculate checksum.

1,627 Views
Claude_Sylvain
Contributor I
Hello,
 
I use CodeWarrior V6.4 for Coldfire.
The target I use is a MCF52223 MCU.
CodeWarrior is running over Windows XP professionnal.
 
The problem happen when using the "Flash Programmer" tool, and can be describe as follow:
 
When using the Flash Programmer tool to calculate a checksum with the option "Compute Checksum Over..."->"Memory Range on Target" selected, and the "Address Range"->"Start: 0x" set to a value other than "00000000", the operation fail all the time.
When this value is set to "00000000", all is working correctly.
 
Is it possible that this tool can only calculate checksum starting from 0x00000000 !?
Or, is there something I am missing ?
 
 
Claude.
Electro-Technica inc.
 
 
Labels (1)
0 Kudos
2 Replies

236 Views
CrasyCat
Specialist III
Hello
 
I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.
 
CrasyCat
0 Kudos

236 Views
Claude_Sylvain
Contributor I
Hello CrasyCat,
 
I just submited a service request for that issue.
 
Thank you.
Claude.
Electro-Technica inc.
 
0 Kudos