I am using Development Board M5213EVB and external debugger USB-ML-CF (vendor P&E Microcontroller Systems). I have a problem while loading sample program code to the target controller. I have performed the following steps:
1. Installed CodeWarior (version 6.2,build 11) , included to KIT.
2. Compiled the sample project “M5213EVB CONSOLE-SRAM” from catalog (CodeWarrior_Examples)\M5213EVB.
3. Pressed button [ |> ] to debug the program. CodeWarior began to load the program to target controller, but loading process broke with the error message “ PEMicro Protocol Plugin: An Error occurred while trying to write memory” or error message “ Could not set PC to entry point”
What I have to do to solve this problem?