AnsweredAssumed Answered

Why is OnMasterBlockSent not called?

Question asked by Thomas Dowad on Jun 4, 2013
Latest reply on Oct 19, 2013 by Vinod Ganesh

Codewarrior 10.4

K20 MCU

 

I am setting up the I2C port using PE. Master Mode. I call I2C1_MasterBlockSend() to send 4 bytes with SendStop = 1. It returns ERR_OK. I have a breakpoint in the OnMasterBlockSent event handler. Never gets there. The event code is being generated, and the Event Mask has the event enabled.

 

Any ideas of what other factor is preventing the event function to be called?

 

TIA

Outcomes