I.MX 281 BOOT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX 281 BOOT

1,225 Views
annyli
Contributor II

How to generate a .sb file for a bareboard program.

we do a bareboard program for the IMX281 platform. We want to download and boot it from SPI flash.

Could you introduce the process and provide an example for reference?

Tags (1)
0 Kudos
5 Replies

913 Views
GraceH
Senior Contributor II

You can reference the code of imx_28_obds_release_v1_0.tar.gz.

It is standalone On-Board Diagnostic Suit for the i.MX28.

After you decompress the package, you can find "User Guide for i.MX28 On-Board Diagnostics Suite (OBDS)"

You can download the package from www.freescale.com

i.MX281 Product Summary Page

Lab and Test Software (1)

IMX_OBDS : On-Board Diagnostic Suit for the i.MX28.

Size (K): 10097 Format: gz Rev #: 1 Modified: 3/3/2011

0 Kudos

913 Views
FrankLi1z
NXP Employee
NXP Employee

You can use tools elftosb to generate sb file. You need write db file. You can reference linux-bootlets.

elftosb already release source code in linux public release.

0 Kudos

913 Views
annyli
Contributor II

Hi, thank you for your proposal. Do you know how to write the db file? We find some db file source examples, but we don't know what the meaning of the codes,  can you offer some reference to write the db file? You know in the db file, there are many addresses, how should we find the address? and what they are used for?

0 Kudos

913 Views
YixingKong
Senior Contributor IV

Anny, if you got answered, please click Correct Answer/Helpful Answer.

Thanks,

Yixing

0 Kudos

913 Views
annyli
Contributor II

Tel: 0510-8029 5234

Email: lijunmei886@163.com

Anny Li

0 Kudos