Hi,
I'm using an 9S08AC128 with an external 4.000MHz canned oscillator, and require a bus clock of 16.000MHz. I've assumed I will need to switch to FEE mode, with N=16 and R=2.
To test my overall project I have a 32.000MHz oscillator attached, creating a 16.000MHz bus clock.
ICG_Init mov #%01010000,rICGC1
mov #%00000000,rICGC2
rts
The above code works fine. I have a timer generating a 1Hz signal that flashes a LED and it's quite accurate as you would expect. Now it's time to swap over to the 4.000MHz oscillator.
Page 201 of the Reference Manual provides an example that generates a bus clock of 20 MHz from a 4MHz crystal. The code example is:
ICG_Init mov #%01111000,rICGC1
mov #%00110000,rICGC2 ;N=10, R=1
rts
When I run this code I get a bus clock substantially below 20 MHz (visible by a very slow flashing LED). My plan was to then change ICGC2 to N=16 and R=2 to generate my 16.000MHz bus clock.
Curiously page 202 of the same Reference Manual gives a different value for ICGC1 than the previous page for the same example, and I suspect that's a typo.
Any suggestions about what I have overlooked?
David
Hello David,
Using a 4MHz external oscillator, the combination N = 10, R = 1 should correctly generate a 40 MHz DCO frequency, and a 20 MHz bus frequency. This is on the upper DCO frequency limit. It might pay to initially leave R at the default value of 2 whilst setting up FEE mode. After lock has occurred, you would then set R = 1 as a separate process. This will avoid the possibility of overclocking the MCU prior to lock occurring.
For a bus frequency of 16 MHz, the only combination that will work is N = 8, R = 1. If you attempt to set N = 16, this will exceed the maximum DCO frequency limit, and lock will not occur.
Since you are using an external oscillator, rather than a crystal, it is unnecessary to set bit-5 of ICGC1. This will free up the XTAL pin for GPIO use.
Regards,
Mac