Hi all,
we want to connect a 4,3" Display ( 480x272 ) to i.MX28 Eval Board with WinCE6.
The hardware we could check with a "eboot_ivbt". The boot logo is correctly shown on 4,3" Display
during eboot.
Inside FreeScale WinCE6 BSP there a two display drivers :
LMS430HF02 : "GUID"="{1ED47D96-6842-4c20-8705-BF05AD0DFC33}"
43WVF1G : "GUID"="{83A0FF68-78BB-4DF5-8DEB-077961EE75BC}"
I have modified the LMS430 driver for our DOTCLK_... & PIXEL_CLOCK data and have set :
"GUID"="{1ED47D96-6842-4c20-8705-BF05AD0DFC33}".
Over DEBUG-UART it is shown that LMS430HF02 is loaded correctly.
But sometimes only VSYNC or sometimes only HSYNC is output. Sometimes the data are not output.
( measured with oscilloscope ). I have never seen a correct picture.
Our question : What can we do to get the LMS430 driver inside WinCE6 BSP working ?
Thank you
Best regards
Martin
Chang
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
Chang
We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to
reply with an update to this discussion.
Thanks,
Yixing
Chang
We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the
issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.
Thanks,
Yixing