AnsweredAssumed Answered

problems with demo mfs_usb

Question asked by simonepuschmann on May 23, 2013
Latest reply on Jun 3, 2013 by simonepuschmann

Hello,

 

I'm using the TWR-K60D100M Tower Module with cw 10.3 and MQX 4.0 and try to run the example mfs_usb.

I use a 8GB usb stick on the TWR_SER Module

 

When I use the command "dir" I get the message "Error, file system not mounted"

 

In debug mode I can see, that I never reached line 224 in USB_Task.c (usb_filesystem_install...)

It looks as if waiting for an event. I try to connect and disconnect the usb stick, but nothing happend.


Does anyone have an idea what I'm doing wrong.

 

 


Outcomes