Hi all
I am using IMX6Q Nitrogen6x Board from Boundary Devices. I have an BMP Image to be displayed onto HDMI Display, whenever u-boot starts. I have enabled BMP feature in U-Boot and a script is employed to automatically display the image when u-boot starts. When I power cycle the board (remove the power connector and plug it back), I am able to see the image. But when I issue a reboot after booting into ubuntu, and enter u-boot, this image is not getting displayed. I feel my Frame Buffer is messed up when I reboot. Has anyone come across this issue? If so, let me know how did you overcome it. Any pointers or suggestions are much appreciated. Also let me know if I should suspect HDMI registers (As per my understanding upon reboot, all hdmi registers are taken to reset state, which is same as just powered state).
FYI:
The version of u-boot that I am using is the "production" branch from boundarydevices/u-boot-imx6 · GitHub
Regards,
Balaji V
Finally could resolve this problem. Please refer to the comments in the following link.