Can i use Hynx memory and flash with imx6 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i use Hynx memory and flash with imx6 processor

742 Views
raghavendraanja
Contributor II

Hi all

i need to use the memory and flash from Hynx with part numbers

H5TQ4G63MFR-*xxC-Memory

HY27UF084G2M-Flash


Has any one used this with iMx6.


What is the reliability? i have chosen this keeping in the cost of my product.

Labels (1)
0 Kudos
2 Replies

538 Views
weidong_sun
NXP TechSupport
NXP TechSupport

hello,raghavendra,

       Please send their datasheets to me ! Let me check them . My email : weidong.sun@freescale.com

Thanks,

Weidong

0 Kudos

538 Views
weidong_sun
NXP TechSupport
NXP TechSupport

hello,raghavendra,

      I checked the datasheets of memory and nand flash, They are both OK for i.mx6. Only please note DDR3 memory capacity, on MX6 EVK, it is 2Gbit, yours is 4Gbit, So software engineer will re-configure u-boot/board/freescale/mach-mx6q/flash_header.S, which is configure memory controller . Reference document is Reference manual.

Regards,

Weidong

0 Kudos