AnsweredAssumed Answered

PE in 10.4, how to get Component Inspector to show port?

Question asked by Thomas Dowad on May 14, 2013
Latest reply on May 15, 2013 by Thomas Dowad

I created a new bareboard project, with PE enabled. PTA was initially configured with the TSI (I did nothing to cause this, it just came up that way). I needed to use some PTA pins for GPIOs, so I added the GPIO init component. This apparently worked and I was able to set the initialization parameters for PTA GPIOs. But the TSI was still there (for the other pins I presume) and so the icon inside the PTA box (on the chip graphic) displays a blue circle with some dots on it. The software knows there are multiple components for that port. Here's the problem. On all other ports, I can click on the box/graphic (on the chip graphic) and the component inspector will show the component. But for this one port where there are two components, it won't do that. No change. I have been searching menus for another way to select PTA but cannot find it.


So need a way to select a component in Component Inspector, other than clicking on the chip graphic.

Outcomes