Power-On delay with MMPF0100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power-On delay with MMPF0100

Jump to solution
1,501 Views
ottawa-imx6
Contributor IV

Hello everyone...,

We are designing based on the sabresd reference and use of the MMPF0100.

From what I can see, almost ALL commercial 'smart' devices have some form of power-on delay (2-4 seconds) to avoid powering up the system inadvertently. Strangely though, this very capable PMIC offers everything except this capability.


Does anyone have any suggestions for implementing a power-on delay with the MMPF0100 PMIC?

Thanks

Brent

Labels (2)
Tags (2)
1 Solution
834 Views
admin
Specialist II

From AnandBalakrishnan:

Hi Brent,

Unfortunately neither the PMIC nor the processor has built-in circuits to support this type of delay. You can use the below circuit to create a delay.

startup delay.jpg

Regards,

Anand

View solution in original post

0 Kudos
5 Replies
834 Views
ottawa-imx6
Contributor IV

Hi Everyone, Just following up on this older post. I believe that the processor might actuall contains logic to adjust the PMIC on/off time delay. I haven't tested it yet since our device already employs the required additional circuitry for the delay, but this may save someone else the added cost of this additional circuitry.....if it does work.

Grant... What do you think? I don't remember seeing this in the earlier versions of the documentation, so it may be simply newly documented.

Check out

57.9.10 SNVS_LP Control Register (SNVS_LPCR)

Screen Shot 2015-01-28 at 3.58.44 PM.png

834 Views
admin
Specialist II

Anandkumar Balakrishnan

Anand, can you weigh in on this?

Thanks,

Grant

0 Kudos
835 Views
admin
Specialist II

From AnandBalakrishnan:

Hi Brent,

Unfortunately neither the PMIC nor the processor has built-in circuits to support this type of delay. You can use the below circuit to create a delay.

startup delay.jpg

Regards,

Anand

0 Kudos
834 Views
jh_zhao
Contributor I

Hi

Is there a clearer picture?

Regards,

Jihua.

0 Kudos
834 Views
ottawa-imx6
Contributor IV

Thanks very much Anand, this will definitely help move us forward.

Regards

Brent

0 Kudos