How to change the default Camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change the default Camera

522 Views
phillipchen
Contributor I

I have two EVBs, which are MCiMX6Q-SDP and MCiMX6Q-SDB. I installed the camera, which comes from the MCiMX6Q-SDP, on the front camera port (J9)of the MCiMX6Q-SDB. Because the default camera is the rear camera (J5), I still can't start the camera function after I installed the camera on the MCiMX6Q-SDB. How can I change the default camera?

Thanks

Best Regards,

Phillip

Labels (2)
0 Kudos
0 Replies