AnsweredAssumed Answered

Flash programming for production

Question asked by Leslie Yang on May 13, 2013
Latest reply on Apr 23, 2014 by takaoyamada

Hi,

 

Here is my approach that I'm using now to program code into MCU internal flash:

(1) Build the bootloader project (in CW10.4)

(2) Run "Debug" bootloader project

(3) Disconnect CE10.4 and target device(P&E multi-link)

(4) Connect target device with PC via USB cable

(5) Targer device look as a mass storage from PC

(6) Build the application project and generate .S19 file

(7) Copy .S19 file from PC to mass storage

(8) Power recycle the target device

 

I am search for another approach to program the bootloader and application code into MCU interanl flash.

The application note "AN3967_How_to_write_Flash_Programming_Applets.pdf" looks good, but there is not "HC08" or "RS08" directory under "{CodeWarriorInstallDir}\MCU\bin\plugins\support\Flash_Programmer\".

Maybe it is because I only chose "Kinetis" during install CW10.4?

 

Is there another approach to program the code info MCU flash?

 

Thank you.

 

Leslie

 

----

IDE: CodeWarrior 10.4

MQX 4.0

 

MCU: PK60DN512VLL10

MASK: 2N22D

 

MCU: MK60DN512VLL10

MASK: 4N22D

 

Outcomes