Broken links in L2.6.35_11.03.00_ER_source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Broken links in L2.6.35_11.03.00_ER_source

1,173 Views
aldobiziak
Contributor II

Goodmorning everybody,

I've downloaded LTIB version L2.6.35_11.03_ER_source_bundle.tar.gz and I've tried to install it by the basic commands:

./ltim -m config

./ltib

When I set QT installation (with or without X11 support), ltib can't find link for sources:

#./ltib

...

Try qt-everywhere-opensource-src-4.6.0.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/qt-everywhere-opensource-src-4.6.0.tar.gz.md5:

23:55:55 ERROR 404: Not Found.

Try qt-everywhere-opensource-src-4.6.0.tar.gz from the GPP

http://bitshrine.org/gpp/qt-everywhere-opensource-src-4.6.0.tar.gz:

23:55:56 ERROR 404: Not Found.

Can't get: qt-everywhere-opensource-src-4.6.0.tar.gz at ./ltib line 790.

So, URL is broken.

I've tried to download qt-everywhere-opensource-src-4.6.0.tar.gz from web and copy it in /opt/freescale/pkgs. But its compilation fails:

#./ltib

...

  The specified system/compiler is not supported:

      /home/user/Documents/L2.6.35_11.03_ER_source_bundle/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/mkspecs/qws/linux-g++-mx

   Please see the README file for a complete list.

error: Bad exit status from /home/user/Documents/L2.6.35_11.03_ER_source_bundle/ltib/tmp/rpm-tmp.96334 (%build)

RPM build errors:

    Bad exit status from /home/user/Documents/L2.6.35_11.03_ER_source_bundle/ltib/tmp/rpm-tmp.96334 (%build)

Build time for qt-embedded: 0 seconds

Failed building qt-embedded

So, where is a valid repository url for qt-everywhere-opensource-src-4.6.0.tar.gz ?

Labels (1)
0 Kudos
3 Replies

638 Views
robby
NXP Employee
NXP Employee

please check this link  https://community.freescale.com/thread/300825 to see if it's helpful.

0 Kudos

638 Views
aldobiziak
Contributor II

Your linked page shows how to install Qt manually instead of using "ltib - m config".

But the page is not clear: where is the link to download "mkspec package"?

0 Kudos

638 Views
Yuri
NXP Employee
NXP Employee

The following may be helpful :

https://community.freescale.com/docs/DOC-1481

0 Kudos