mohamedkalilullah

Re: iMX6 and eMMC 4.5

Discussion created by mohamedkalilullah on Apr 22, 2013
Branched from an earlier discussion

Hello,

 

     MMC 4.4.1 is using in Customized imx6 board as boot device, after booting android (R13_04_ga), media files are detecting from MMC, SD, and USB taking long time also all applications taking long time for loading.

 

for eMMC is selected as default storage, changes are done in "vold.fstab" file,

if i select SD card as boot device, media files are detecting very fast, what are the changes i have to done for MMC?

 

Regards,

Kalil

Outcomes