Andre Ribeiro

MC908QB8 board design questions

Discussion created by Andre Ribeiro on Jul 10, 2007
Latest reply on Jul 12, 2007 by bigmac
Hi all,
 
I'm new with the HC08 and its MON08 programming interface. Normally I work with the HC12 (BDM).
Thing is that I need to design a new board with the MC908QB8 (16 pin) and looking at the MON08 interface, it seams that 6 pins of the MCU will be used for the MON08 interface... I need to use those pins for the application so my questions are:
1) What is the best way to program/debug the MC908GB8 without loosing the MON08 6 pins of the MCU?
2) Is it possible to continuing to use all the MCU pins for application purposes instead of MON08 interface without using additional signal switching hardware?
 
It's a pity that the MC9S08QG8 is low voltage...
 
Thanks in advance for your comments,
 
Andre

Outcomes