Hi all.
I wonder if exist another way to flash the 51CN MCU without using CodeWarrior, or a external BDM?. Only the embedded OSBDM on the tower module.
Thanks!
Ángel
if you use classic CW, you can use hiwave debugger to download s19 file to chip. it can run without open CW ide.
you can also use P&E standalone programmer.
Hi Jun.
Thanks for you answer, but I'm using CW 10.3, and the hiwave debugger doesn't work on Win7 x64 (it miss some dll's -> osbdm.dll)
Thanks,
Ángel.