Enable SDHC Interface in IFC NAND boot mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable SDHC Interface in IFC NAND boot mode

921 Views
bfac
NXP Employee
NXP Employee

Hello!

We are using P1010 with BSP v1.3, tests done on fsl rdb board.

When booting from IFC the SDHC interface is disabled, this seems to be a known limitation.

There are documents explaining how to enable SDHC interface on SPI boot mode.

Is that also possible on IFC boot mode?

We only need to access SDHC interface after boot, just for data storage purposes.

As per previous consultation with product engineering, it doesnt seem we have a hardware chip limitation for using both interfaces at the same time.

The kernel boot log is below.

Thanks!

Bruno

NAND boot...
  NAND boot... WARNING: ECC not checked in SPL, check board cfg
 
 
  U-Boot 2011.12-00064-gbfb0c9a (Jun 15 2012 - 00:25:55)
 
  CPU:   P1010E, Version: 1.0, (0x80f90010)
  Core:  E500, Version: 5.1, (0x80212151)
  Clock Configuration:
         CPU0:800  MHz,
         CCB:400  MHz,
         DDR:400  MHz (800 MT/s data rate) (Asynchronous), IFC:100  MHz
  L1:    D-cache 32 kB enabled
         I-cache 32 kB enabled
  Board: P1010RDB
  I2C:   ready
  SPI:   ready
  DRAM:  DIMM 0: is not a DDR3 SPD.
  16 MiB (DDR3, 32-bit, CL=5, ECC off)
  Flash: 32 MiB     <------
  L2:    256 KB enabled
  NAND:  32 MiB
  ....
 
  linux kernel loading:
 


  loop: module loaded
  fsl-ifc ffe1e000.ifc: IFC Set Information for bank 0
  NAND device: Manufacturer ID: 0xec, Chip ID: 0x75 (Samsung NAND 32MiB 3,3V 8-bit)                  <--------- NAND is detect correctly.
  Scanning device for bad blocks
  Bad eraseblock 222 at 0x000000378000
  IFC NAND device at 0xff800000, bank 0
  ...
  EDAC MC: Ver: 2.1.0
  sdhci: Secure Digital Host Controller Interface driver
  sdhci: Copyright(c) Pierre Ossman                 <-----------------  SDHC not detected.
  usbcore: registered new interface driver usbhid
  ....

0 Kudos
0 Replies