Hello,
i need to generate these clock frequencies in MCF54415 cpu
Core System & SDRAM Clock | 250MHz |
Peripheral Clock | 125MHz |
FB Clock | 100MHz |
USB Bus | 60MHz |
NAND Flash Controller | 80MHz |
eSDHC Clock | 40MHz |
How to set the reference clock for the same.
Thanks in advance.
This Forum is titled as being for "general questions regarding community interaction and/or collaboration". You should be asking this in the ColdFire Forum.
The Admins may move this question there for you.
Tom