AnsweredAssumed Answered

FRDM-KLZ25Z Will not connect in IAR enviornment.

Question asked by Dave Grissom on Apr 12, 2013
Latest reply on Aug 30, 2013 by Derek Snell

I have installed PE Micro Drivers.  I do note that in my device drivers under Jungo, I only see one listing, that of WinDriver.  Someone else told me they had two entries under Jungo.  When I bring up my IAR ARM V6.50.2, load an example program made for IAR (pwm_led) and try to move to debug, I get an window telling me "port: Undetected. Disconnect/Connect USB cable. Click Refresh List."  No matter select after this, I can not connect.  I am sure I have the latest drivers from PEMicro.  Anybody have this problem or an idea how to fix it?  I am plugged into the SDA connector.  My PC does recognize the KL25Z as an SD card and displays the directory.  The green LED is flashing at about a half second on and half second off.  The multicolor LED changes color when I move the KLZ25 as expected. 

Outcomes