AnsweredAssumed Answered

iMx28 wpa_supplicant

Question asked by vikranthreddy on Apr 9, 2013
Latest reply on Jul 23, 2013 by Jason Harper
Branched to a new discussion

Hello all,

 

I've been trying to add wpa-supplicant to Linux-BSP build for iMX28 (L2.6.35_1.1.0_130130_source.tar.gz). It doesn't show up in LTIB build configuration menu.

 

I've tried to build manually with following command.

./ltib -m prep -p wpa_supplicant

 

It gave an error in unzipping the wpa_supplicant package. When I checked the pacakges directory in /opt/freescale, the size of the file is 1044 bytes, which doesn't see correct.

 

Where can I find the right source for wpa-supplicant package for iMx28 Linux-BSP? Or do I need to port it from x86 base wpa_supplicant from below link ?

 

Linux WPA Supplicant (IEEE 802.1X, WPA, WPA2, RSN, IEEE 802.11i)

 

Regards

Outcomes