AnsweredAssumed Answered

Connectivity of  10.1” 1024 x 768 XGA display (Ref.:MCIMX-LVDS1)

Question asked by siuho on Apr 8, 2013
Latest reply on Apr 9, 2013 by siuho

Hi,

 

I have bought a 10.1” 1024 x 768 XGA display (Ref.:MCIMX-LVDS1) which stated the display is dedicated for i.MX53.

Regarding the processor, I had bought a development board from Digi (Part No : CC-WMX53-LX) that has featured an i.MX53 processor and the LVDS port connector is DF14-30P-1.25H(25).

I was trying to connect the i.MX53 development board to the display through the LVDS port where both the connectors are not compatible.

 

I would like to ask if anyone knows the model number of the LVDS connector at the display panel so I could be able to make an adapter accordingly.

 

Many thanks.

 

Kind Regards,

 

Siu Ho

Outcomes