I have completed my application and found running fine from codewarrior IDE into the Kwikstik k40. But once when I remove or power of the board the application is not running.
Now I want to port it permanently to the Kwikstik k40 board.
What to do?
Anyone please.........
THank you for your information friend. I did the same before (Clean, rebuild and downloaded it.). But in power on reset the application is not running, once again I have to debug the same thru codewarrior IDE. If u have any solution pls reply me soon.
Are you using the FLASH build? The RAM build will obviously not run after a reset.
On the "Project/Build configurations/Set active" menu, hopefully there is a Flash build of the project.
Clean, rebuild and download it.