AnsweredAssumed Answered

Debug serial port on SABRE outputs rubbish

Question asked by emil on Mar 19, 2013

I've just copied the images to the eMMC with the MFGTool using this option in the cfg.ini-file:

 

board=SabreSD

name=i.MX6DL-SABRESD-eMMC

Description:Download the u-boot, kernel and Linux rootfs to the eMMC

 

I have a usb cable conected to the USB to UART port and I can see things happening on the terminal. All of a sudden when booting up linux i start getting rubbish on the serial port. It seems like the bootup routine is doing something with the serial port. Also, I would like to know how to configure the boot environment variables so that I can get the video output on the touchscreen (which comes with the SABRE Smart Devices kit).

 

I'll attach the log from the serial output.

 

Thanks.

 

Original Attachment has been moved to: putty2013-03-19-104503.log.zip

Outcomes