CW 10.3
MQX 3.8.1
MCU: PXN20
CW is issuing compilation errors in mqx.h. For example, the first few starting at line 149 are:
typedef uint_16 _task_number; // (expression syntax error)
typedef uint_32 _task_id; // (expression syntax error)
In all, there are 62 errors shown in mqx.h, of which 59 are (expression syntax error)s, the majority being in forward declarations of functions.
There are 2 errors of: (';' expected) and 1 error of: ( ')' expected)
Is there a comprehensive list dscribing the prescribed order of include files?
Any help would be greatly appreciated.
Thanks in advance,
ED
Message was edited by: EDWARD DAROSA Solved by reordering includes.
Hi Edward Darosa,
what did you build? An application , bsp , an example? My first guess would be missing compiler path in the project options.
Regards,
MartinK
MartinK,
I am building an application, actually one I inherited, porting from an old mqx version.
Thanks,
ED