AnsweredAssumed Answered

GSTREAMER RECORDING VIDEO WITH AUDIO

Question asked by shanmugamsundar on Mar 10, 2013
Latest reply on Mar 15, 2013 by shanmugamsundar
Branched to a new discussion

hi all,

 

      i am using i.MX535qsb board, i am using camera interface application in that, i need to record the video with audio enabled, for that i am using the below gst command

 

COMMAND:

 

gst-launch mfw_v4lsrc fps-n=30 capture-width=1280 capture-height=720 capture-mode=4  ! queue ! mfw_vpuencoder codec-type=0 ! mux. alsasrc ! mfw_mp3encoder bitrate=64 ! queue  ! mux. avimux name=mux ! filesink location=shan3.avi sync=false

 

     In the above command the video is recording, but the audio is not coming, i want to change any parameters? can any one help me

 

NOTE:

I am using MOVIE player to open the recorded file in that it shows no audio.

But, if i use GNOME player to open the video the sound is coming, but the video runs very fast.

 

Thanks,

shan

Outcomes