Hi,
I have been using the tbdml for a long time in the 9S12 with great success. The other day I came across an old M5213Badge board that I would like to get some code into and use.
The tbdml is supposed to support coldfire V1, but this badge board has a 26-pint connector, which I suppose is Jtag. The tbdml pod has a standard 6-pin bdm connector. Are there pins on this connector that will connect to the bdm module inside the coldfire? Sorry if this is a dumb question but I am not familiar with jtag.
Nigel Johnson
Well your basic problem is MCF5213 is a V2, not a V1, therefore it has a 26 pin BDM connector and is not supported by TBDML.