AnsweredAssumed Answered

Linux won't boot on i.mx53 board

Question asked by Bernard Mentink on Mar 6, 2013
Latest reply on Mar 15, 2013 by Lily Zhang

Hi There,

 

I am having trouble getting the linux kernel to boot a custom board based on the ARD board.

 

I am not sure what text is outputted by the bootloader and what by the kernel starting up ..

 

Here is the output from the serial console:

 

Thanks,

Bernie

 

Mem Start= 1879048192 Mem Size= 268435456

## Booting kernel from Legacy Image at 70200000 ...

   Image Name:   linux-2.6

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3430768 Bytes =  3.3 MB

   Load Address: 70200000

   Entry Point:  70200000

   Verifying Checksum ... OK

   XIP Kernel Image ... OK

OK

 

 

*** Just entered do_bootm_linux func ...

 

 

 

 

## Transferring control to Linux (at address 70200000) ...

 

 

 

 

*** Setup_start

*** hdr.tag: 54410001

*** hdr.size: 00000005

 

 

*** Setup_revison_tags

*** hdr.tag: 54410007

*** hdr.size: 00000003

*** revision: 00053121

 

 

*** Setup_memory_tags

*** 0 hdr.tag: 54410002

*** 0 hdr.size: 00000004

*** 0 u.mem.start: 70000000

*** 0 u.mem.size: 10000000

 

 

*** Setup_commandline_tags

*** hdr.tag: 54410009

*** hdr.size: 0000000b

*** cmdline: 70000138

Starting kernel ...

 

 

 

 

Ready to jump to OS ...

machid 00000bc2

boot_param 70000100

 

 

 

Outcomes