Is there a PE tutorial for MQX.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a PE tutorial for MQX.

Jump to solution
635 Views
barbercolman
Contributor III

Is there a PE tutorial for MQX? All the examples I have found are non mqx. One of the questions I have is under the MQX directory is see

C:\Freescale\Freescale_MQX_4_0\demo\pe_demo

C:\Freescale\Freescale_MQX_4_0\mqx\examples

C:\Freescale\Freescale_MQX_4_0\usb\host

Which of these three examples do I use for a PE based project that user MQX and can act as a USB host.

Thanks

I also looked in the PE forums but did not see a good answer so I posted here.

Tags (3)
0 Kudos
1 Solution
382 Views
dereksnell
NXP Employee
NXP Employee

Hi Dale,

Yes, there is a tutorial for using Processor Expert (PEx) with MQX. It’s included in the documentation installed with MQX. You will find it at \Freescale_MQX_4_0\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf

The pe_demo is a demo application for using PEx in your BSP, and is discussed in the tutorial above.

View solution in original post

0 Kudos
1 Reply
383 Views
dereksnell
NXP Employee
NXP Employee

Hi Dale,

Yes, there is a tutorial for using Processor Expert (PEx) with MQX. It’s included in the documentation installed with MQX. You will find it at \Freescale_MQX_4_0\doc\tools\cw\FSL_MQX_in_CW_10_x.pdf

The pe_demo is a demo application for using PEx in your BSP, and is discussed in the tutorial above.

0 Kudos