Using the GPIOs on iMX535.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the GPIOs on iMX535.

2,224 Views
dimitardyakoff
Contributor I

The set up:

I have i.MX53 module mounted on a custom board. On the custom board there are peripherals such as GPS, GPSR module, LEDs etc. It is running Linux 2.6.35.3.

The goal is to start the GPS module. To do so I have to set logical high on certain pins (GPIO2_31 and USER_UI2).

Under the directory /sys/class/gpio/ I have:

gpiochip0

gpiochip128

gpiochip160

gpiochip192

gpiochip32

gpiochip64

gpiochip96

As I understand from the from the documentation the number after gpiochip is determined by the formula "<GPIO Instance – 1> × 32 + <GPIO Port number>" What is  "Instance", the actual pin on the chip? And how to determine the "Port number"?

Lets say that i have configured the GPIO pin. In the documentations is writtren "echo 0 > /sys/class/gpio/gpio199/value" to set the value of the pin.
But this is the result:

root@freescale /$ echo 1 > /sys/class/gpio/gpiochip64/value

-sh: /sys/class/gpio/gpiochip64/value: No such file or directory


Under the /sys/class/gpio/gpiochip64/ directory there is only this:


-r--r--r--1 root root      4096 Jan  1 02:50 base
-r--r--r--1 root root      4096 Jan  1 02:50 label
-r--r--r--1 root root      4096 Jan  1 02:50 ngpio
drwxr-xr-x2 root root         0 Jan  1 02:50 power
lrwxrwxrwx1 root root         0 Jan  1 02:50 subsystem -> ../../../../class/gpio
-rw-r--r--1 root root      4096 Jan  1 00:00 uevent


What am I doing wrong? Any other documentation or example to read?

Source:

i.MX53 System Development User’s Guide (MX53UG Rev.1 3/2011)


P.S. I am new to embedded linux development, any help would be appreciated.


Labels (2)
Tags (1)
0 Kudos
1 Reply

685 Views
RodBorras
NXP Employee
NXP Employee

Dimitar,

You are missing a few steps. See: GPIO access

Regards,

Rod.