USB Stack, bare metal, all versions, supported devices?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Stack, bare metal, all versions, supported devices?

781 Views
gigglerg
Contributor II

Simple question, if the K60 supports USB, why does the supported devices for the bare metal stack not include the K60?  My tower has the K60, I've been building the samples for K70 and the ones I've been using seem to function.  Played with the PLL on some to get it booting.

Can I have an answer on if the K60 is supported because that is series we will be using in project.

Regards,

dc

0 Kudos
4 Replies

540 Views
LuisCasado
NXP Employee
NXP Employee

Hi,

K60 is supported:

device, i.e. : C:\Freescale\Freescale USB Stack v4.0.3\Source\Device\app\cdc\cw10\kinetis_k60

Host, i.e : C:\Freescale\Freescale USB Stack v4.0.3\Source\Host\examples\cdc_serial\cw10\kinetis_k60


Regards,

Luis

540 Views
gigglerg
Contributor II

That's not what it says in their supported device list on website:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB

Which is why I asked.

0 Kudos

540 Views
LuisCasado
NXP Employee
NXP Employee

Hi,

It is in the release notes:

http://cache.freescale.com/files/microcontrollers/doc/support_info/USB_STACK_RELEASE_NOTES_V4.0.3.pd...

In the same link you provided.

Best Regards,

Luis

540 Views
gigglerg
Contributor II

Different link, it's in a PDF at the end but not on download page on website but thanks for answering.

0 Kudos