AnsweredAssumed Answered

Latest u-boot (2013.01) on mx28evk

Question asked by Ruud Commandeur on Feb 27, 2013
Latest reply on Feb 28, 2013 by Fabio Estevam

Hi everyone,

 

I tried to run the latest u-boot-imx on the mx28evk, but this hangs just after startup reporting only 61 bytes of DRAM. This is the debug output it shows:

 

PowerPrep start initialize power...

Battery Voltage = 4.23V

boot from battery. 5v input not detected

Feb 26 201314:24:45

FRAC 0x92925552

memory type is DDR2

                   Wait for ddr ready 1power 0x00820616

Frac 0x92925552

start change cpu freq

hbus 0x00000003

cpu 0x00010001

start test memory accress

ddr2 0x40000000

finish simple test

 

U-Boot 2013.01-10534-gbec0160 (Feb 26 2013 - 15:35:44)

 

CPU:   Freescale i.MX28 rev1.2 at 454 MHz

BOOT:  PHY ID 1 register

I2C:   ready

DRAM:  61 Bytes

 

I followed these steps to create this u-boot version:

 

//Get latest u-boot-imx

git clone git://git.denx.de/u-boot-imx.git

//Set cross compiler environment

export ARCH=arm

export CROSS_COMPILE=arm-none-linux-gnueabi-

export PATH="$PATH:/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/"

export PATH="$PATH:/opt/freescale/ltib/usr/bin/"

//Make the u-boot for the mx28evk

make mx28evk_config

make u-boot.sb

 

 

 

Since the imx28 on the evk requires a secure boot, I took the following extra steps:

 

  • copied the generated u-boot file to the ltib/rootfs/u-boot
  • ran "./ltib -p boot_stream.spec -f" to create a secured bootstream
  • ran "./mk_mx28_sd -u -b /dev/sdc" to create a bootable sd-card

 

Plugged in the sd-card and powered on the board.


My guess is, that the building of the u-boot requires some extra configuration. But from earlier posts I understood it could run "out of the box". Does anyone have an idea what goes wrong here?


N.B. The board itself is OK. If I take the u-boot from the original ltib (2009.08), the startup is OK, showing 128 MB of DRAM.


Regards,


Ruud

Outcomes