AnsweredAssumed Answered

dual camera work at the same time

Question asked by ff on Feb 19, 2013
Latest reply on May 22, 2015 by Nathan Mak
Branched to a new discussion

hi  guys

  i read the imx53 rm .it says

Several sensors can be connected to each of the CSIs. Simultaneous functionality

(sending data) is supported as follows:

• Two sensors can send data independently, each through a different port.

• Only one of the streams can be transferred to the VDIC or IC for on-the-fly

processing, while the other one is sent directly to system memory.

 

i do not understand what does on the fly processing  and sent directly to system menmory means

 

does it mean  when two sensor work at the same time  the preview image  one is sent to the lcd display device   the other is sent to memory

can i  save both of them at the same time

 

best regards

 

Forion

 

 

 

Outcomes