Hello,
I have got a SABRE Lite board and I installed the L3.0.35_1.1.0 U-Boot, kernel and Ubuntu RFS on this system. I want to use OpenGL hardware acceleration in X11. The output of /var/log/Xorg.0.log looks as it should be according to your guidelines. /etc/X11/xorg.conf is also setup as required. However, when I run glxinfo, the output is as follows:
OpenGL vendor string: Mesa Project
OpenGL renderer string: Software Rasterizer
OpenGL version string: 2.1 Mesa 7.11
OpenGL shading language version string: 1.20
Furthermore, all OpenGL applications are running very slowly. What could be the problem? Please find the log and and configuration files attached.
Thanks in advance,
Martin Scherer
Original Attachment has been moved to: xorg.conf.zip
Original Attachment has been moved to: dmesg.txt.zip
Original Attachment has been moved to: Xorg.0.log.zip
Original Attachment has been moved to: glxinfo.txt.zip
I have same issue, any news on how it should be configured. The "Linux Multimedia Framework User Guide" covers the video/audio side. From what I understand the Ubuntu RFS should include the neccesaary Vivante drivers for X11.
This is also my understanding. I can definitely say, that the deb-package gpu-viv that is mentioned in the user guide is installed on my system.