AnsweredAssumed Answered

Sabre SD (MCIMX6Q-SDB) with L3.0.35_1.1.0 Linux BSP?

Question asked by Steve Kwon on Jan 31, 2013
Latest reply on Feb 5, 2013 by Prabhu Sundararaj
Branched to a new discussion

Hi,

 

I'm having issues getting the new L3.0.35_1.1.0 Linux BSP to even boot on my Sabre SDB board.  I've loaded uBoot and it doesn't seem to boot.  So I had to load uBoot from a older release.

 

I've then try to boot the kernel over SD, eMMC and TFTP, but they are all panicking at around the same point.

 

My question is, do you know if the BSP works with a Sabre SD board?

 

Also, do you know if 3D rendering inside Ubuntu is supported with this release?  So I could run a gl app such as glmark2 and get 3D acceleration?

 

Thanks.

 

Steve

 

 

Outcomes