i.MX6 and VFP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 and VFP

Jump to solution
2,952 Views
Rob_iMX6
Contributor II

Hi

Even though some overview documents mention, that the i.MX6 have VFP, the datasheet does not. Since this is an optional module, not mentioning it means "not included".

Therefore: can anybody of Freescale please confirm this and UPDATE the datasheet?

Thanks und regards,

-Rob

Labels (2)
0 Kudos
1 Solution
777 Views
Yuri
NXP Employee
NXP Employee

In section 12.4.2 “Media Processing Engine (MPE - NEON)” :
of the i.MX6Q Reference Manual (IMX6DQRM) :


“The MPE also implements a VFPv3-D32 Floating-Point Unit.”

Also the following provide some details :

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0409e/index.html

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0409e/index.html

View solution in original post

0 Kudos
1 Reply
778 Views
Yuri
NXP Employee
NXP Employee

In section 12.4.2 “Media Processing Engine (MPE - NEON)” :
of the i.MX6Q Reference Manual (IMX6DQRM) :


“The MPE also implements a VFPv3-D32 Floating-Point Unit.”

Also the following provide some details :

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0409e/index.html

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0409e/index.html

0 Kudos