i need your help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i need your help

693 Views
admin
Specialist II

i am in beginning part of code warrior programming. i want to write the c and assembly coding for M9S08SH8. so what are the procedures i need to take to write the program well. i want the many sample code for 8bit M9S08SH8. if u have any material means please give me. u can also send the link which is available this. please help me.

Labels (1)
1 Reply

340 Views
Derrick
NXP Employee
NXP Employee

Hi Sabha,

I highly recommend starting your project using Processor Expert.  This will create a project template into which you should be able to easily write your own code.  Processor Expert can also be used to create initialization and interface software for the MCU's peripherals.

At the risk of patting my own back, I suggest also taking a look at a couple of my own blog entries:

The Bare Metal Enthusiast:

Start at the Beginning:

https://community.freescale.com/community/the-embedded-beat/blog/2012/02/08/the-bare-metal-enthusias...

I can C clearly:

https://community.freescale.com/community/the-embedded-beat/blog/2012/03/06/the-bare-metal-enthusias...

Best Regards,

Derrick