iMX6 DualLite with Micron DDR3 (2 x MT41J128M16HA)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 DualLite with Micron DDR3 (2 x MT41J128M16HA)

Jump to solution
2,084 Views
rafalwegner
Contributor II

Hello everybody!


Is there a chance someone have configuration file (flash_header.S) for iMX6 Dual Lite connected with DDR3 RAM Memory (2 x MT41J128M16HA)

MMDC should be configured for DDR3 x32.

Thanks in advance!

Rafal

0 Kudos
1 Solution
729 Views
arthur_lai
Senior Contributor II

Hi Rafal,

Basically, you need to modify two register fields in the original flash_header.S in order to support 32-bit DDR3.

1. Change the memory bus size to 32-bit by set DSIZ on MMDC1_MDCTL register to 1.

2. Disable the ODT on higher 32-bit by clearing MMDC2_MPODTCTRL register.

Arthur

View solution in original post

0 Kudos
1 Reply
730 Views
arthur_lai
Senior Contributor II

Hi Rafal,

Basically, you need to modify two register fields in the original flash_header.S in order to support 32-bit DDR3.

1. Change the memory bus size to 32-bit by set DSIZ on MMDC1_MDCTL register to 1.

2. Disable the ODT on higher 32-bit by clearing MMDC2_MPODTCTRL register.

Arthur

0 Kudos