Steps followed
1. Tried to boot Redboot from MMC
2. used serial port and following command to load Linux image (zImage)
load -r -b 0x100000 -m xmodem
Redboot now is ready to receive data and printing out character “C” continuously. To send a file, click on “Transfer -
> Send File -> Xmodem (under Protocol) -> Browse”, choose the file to download and then click on “Send”.
Ymodem can also be chosen for download.
3. Then tried " fis Create zImage " to load this image on to Flash.
but this command is giving following error.
... Read from 0x07ee0000-0x07eff000 at 0x00060000: .
... Read from 0x07ee0000-0x07eff000 at 0x00060000: .
... Read from 0x07ee0000-0x07eff000 at 0x00060000: .
Can't find an empty slot in FIS directory!
So can someone help me in this regard.
Solved! Go to Solution.
have you try to "fis init" first?
Hello Jimmychan,
yes initially i tried this Fis init and then tried to create. Even then it didnt worked.
But today i tried that Fis init and then Fis create, it worked correctly.
Thanks for your input.