AnsweredAssumed Answered

CW 10.3 Compilation Latency on Network drive

Question asked by Philippe Borghini on Jan 20, 2013

Hello

 

I have just installed the CW 10.3 on Windows 7 64bits. Works fine execpt the following point which I can not understand perfectly.

When the project (for ex. the attached project) is installed on local drive it is compiles in around 9s...not so fast but ok I can live with that

When same project is installed on my Network drive attached to LAN running at 100Mbps effective troughput is compiled in more than 40s which is just unacceptable in development phase.

 

I have tried to stop Antivirus, and Firewall -> no change

 

Is there any configuration I have to do to optimized such bahaviour ?

 

Thanks in advance for your help

 

Philippe

Original Attachment has been moved to: TEST_1.zip

Outcomes