Hi, my name is J. Efren Rodriguez and I have an issue with Code Warrior 10.2. My software works ok but its no possible to navigate in it.
The code compiles, generate the binary files and also runs in the pcb board I designed but I can navigate in the code.
Let me explain....
The open declaration or F3 funtions doesnt do anything.
I open the c file, main in this case, select the port B define and press F3. Nothing happens. It is in all the funtions, defines or subroutines. When I download the code in my pcb board,it works right
Could anyone explain me the linker paths I must check to be able to navigate?
Thanks in advice.
Solved! Go to Solution.
Hello,
this sounds like an issue with the Eclipse indexer. Have a look at
Fixing the Eclipse Index | MCU on Eclipse
This probably will help.
Hello,
this sounds like an issue with the Eclipse indexer. Have a look at
Fixing the Eclipse Index | MCU on Eclipse
This probably will help.