AnsweredAssumed Answered

i.mx6 LCD support

Question asked by Max Chou on Jan 16, 2013
Latest reply on Jan 28, 2013 by Max Chou

Hi  All

 

I try to use DISP0 interface to turn on a 1920x1080,

I can't get the correct display,

so I measure the pixel clock,

it is 148.5MHz,

but it seems unstable,

when I set it to 1280x720(74MHz),and 1360x768(85MHz)

the clock looks good,

I could get the correct display,

so I have the below question,

what is the max pixel clock out of DISP_CLK ??

Could I use it to support a 1920x1080 panel ?

 

Sincerely,Max Chou

Outcomes