Hi,
i have trouble creating a library for Kinetis MCU in CodeWarrior 10.2.
My first attempt was to create a new project using the Bareboard project wizard. On the devices page there ist an Option to choose the Project Type/Output, but the Library-Option is greyed out. What is going wrong here?
The second attempt was to change the Linker Output Type to "Library". The project compiles successfully, but I don't get a lib file anyway.
Can anybody give me some hints?
Regards,
Georg
Solved! Go to Solution.
Libaries are supported in the wizard with MC10.3 (final release). It was not yet in the 10.3 beta.
For the ARM gcc compiler, the needed steps are described here: A Library with ARM gcc and Eclipse | MCU on Eclipse
Hi Erich,
thanks for your answer. I'm trying to use the tutorial you posted but have Problems with step 4. If I click the Artifact Type dropdown there is no entry, so I can't choose anything. Can you help me on this?
When will CW 10.3 final be released?
Hi,
I finally downloaded CW 10.3, now my library works fine.
Thanks to both of you!
Georgs