I plugged in this board with the expectation that it would boot off the included SD card and I would see android on the included display. The display shows nothing, nothing comes out the speakers and the FDI driver for Win7 does not work. Are there any tips or instructions to get this thing working out of the box?
Please try demo images from the Web :
In particular :
https://www.freescale.com/webapp/Download?colCode=IMX6_R13.41_ANDROID_DEMO_IMAGE&appType=license&loc...
Turns out on both boards I purchased, the LVDS cables were unplugged. They do not have locking connectors, they are friction fit only. I had to slide the units out of the plastic case reconnect the cables and carefully slide it back into the case. It is kind of a snug fit, and took several tries before I could reassemble the unit without inadvertantly having the LVDS cable slide out of the connector.