SGMII (1000BASE-X) communication between two P1020 processors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGMII (1000BASE-X) communication between two P1020 processors

Jump to solution
4,236 Views
eze
Contributor I

Hello,

A P1020 on one board is connected to a P1020 on another board using the SGMII lines through a SERDES. Since there is no PHY involved I suppose we should call this 1000BASE-X communication. Could you please confirm that the P1020 supports 1000BASE-X? What would be different from building an SGMII driver connected to a PHY?

Thanks in advance,

Eze

0 Kudos
1 Solution
1,457 Views
lunminliang
NXP Employee
NXP Employee

MAC to MAC is possible. Please refer to http://www.freescale.com/files/ftf_2010/Americas/WBNR_FTF10_NET_F0568.pdf for more useful information.

View solution in original post

0 Kudos
1 Reply
1,458 Views
lunminliang
NXP Employee
NXP Employee

MAC to MAC is possible. Please refer to http://www.freescale.com/files/ftf_2010/Americas/WBNR_FTF10_NET_F0568.pdf for more useful information.

0 Kudos