i.mx233 SPI and SDcard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx233 SPI and SDcard

Jump to solution
855 Views
yanir
Contributor II

     I'd like to know if I can use an SD card and an SPI device in the same design with an i.mx23. The SD card and SPI share some pins and the datasheet doesn't mention whether or not they will operate at the same time. I want to boot from an SDcard and access an SPI peripheral during run time. I also want to store data to the SD card while running (logs). Does anyone have any experience with this?

Thanks

Labels (1)
0 Kudos
1 Solution
694 Views
MarekVasut
Senior Contributor I

Yes you can, but on different SPI blocks (there are two identical SPI blocks in MX233). Another options is that while you can not switch between SD/SPI mode at runtime on a single SPI block, you can operate the SD card in SPI mode.

View solution in original post

0 Kudos
2 Replies
695 Views
MarekVasut
Senior Contributor I

Yes you can, but on different SPI blocks (there are two identical SPI blocks in MX233). Another options is that while you can not switch between SD/SPI mode at runtime on a single SPI block, you can operate the SD card in SPI mode.

0 Kudos
694 Views
yanir
Contributor II

Great! Thanks for your response. That should work for me.

0 Kudos