Compositing Engine GC320 on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compositing Engine GC320 on iMX6

Jump to solution
2,097 Views
sunilpatil
Contributor I

How to use 3rd GPU on iMX6 to merge results of the other GPUs?

Please provide pointers to information available.

Thanks.

Labels (1)
1 Solution
840 Views
PrabhuSundarara
NXP Employee
NXP Employee

You use DirectFB or direct gal2d APIs part of the GPU driver.

View solution in original post

0 Kudos
3 Replies
841 Views
PrabhuSundarara
NXP Employee
NXP Employee

You use DirectFB or direct gal2d APIs part of the GPU driver.

0 Kudos
840 Views
ericbeaudoin
Contributor II

Does there is some source code available for the gal2d api?  There is some test application in the linux packages, but it look like the source code of the application is not available... There is a package named gpu-viv-src listed in ltib, but I cannot download it:

./ltib -m prep --pkg gpu-viv-src

Processing: gpu-viv-src

=========================

Build path taken because: build key set, no prebuilt rpm,

Testing network connectivity

OK GPP:

Try gpu-viv-src-1.1.0.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/gpu-viv-src-1.1.0.tar.gz.md5:

16:53:38 ERROR 404: Not Found.

Try gpu-viv-src-1.1.0.tar.gz from the GPP

http://bitshrine.org/gpp/gpu-viv-src-1.1.0.tar.gz:

16:53:39 ERROR 404: Not Found.

Can't get: gpu-viv-src-1.1.0.tar.gz at ./ltib line 802.

Does the source code of the test application that is using the GC320 in fb mode is available?

840 Views
sheldonrucker
Contributor III

Hello Eric,

Were you able to find source code examples for the gal2d API?  I've been looking with no luck.

Thank you,

Sheldon

0 Kudos